Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
Possible Reason for Firmware Failure in 7300

Issue
Firmware upgrade fails in ION Setup and the Device Upgrader, but does not have a specific error code. A general message of "Operation Failed!" or "Upgrade Failed at..."… is given.



Product Line
ION7300

Cause
In this case the firmware version is not compatible with the meter’s Revision. A or B firmware is being installed on a B or A meter. The upgrade fails immediately since the firmware and meter are incompatible.

Resolution
Use the correct firmware version for the revision.
73xx:
Revision A if the last two digits are <= 09
(e.g. PA-0005A123-06)
Revision B if the last two digits are >= 10
(e.g. PA-0005A123-11)

Schneider Electric Egypt and North East Africa

Explore more
Range:
Users group

Discuss this topic with experts

Visit our community and get advice from experts and peers on this topic and more
Explore more
Range:
  • Products Documentation
  • Software Downloads
  • Product Selector
  • Product Substitution and Replacement
  • Help and Contact Center