Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
What is the maximum pulse output rate of PM700P ?

Issue

What is the maximum pulse output rate of the PM700P meter?

Product Line

PowerLogic™ PM700P Series Meter.

Environment

Applications requiring pulse output for energy monitoring, data logging, or integration with external systems such as building management systems (BMS) or SCADA.

Resolution

The pulse output of the PM700P meter can operate at a frequency of up to 9.8 Hz.

Schneider Electric Egypt and North East Africa