Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
Improvement to the Stability of the Input Data for the 170AAI03000

Issue
This Resolution is to inform users of 170AAI03000 analog input modules that the stability of the input data has been improved.


Product Line
Momentum
170AAI03000


Resolution
Typically, input data from any of the inputs would continuously fluctuate up to +/- 11 counts.
Modifications have been made to the module to improve the stability of this data.

Units affected are:

  • 170AAI03000 modules with a PV05 or less.
  • 170AAI03000 modules with a PV06 or higher have this modification that provides improved input data stability.
There are no changes to the specifications of this module.