Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
This FAQ has been written for NEAL (North East Africa and Levant) region. If you are looking for information for another region, please select the correct country from the top-left dropdown in the page and 'Navigate to Browse FAQs' in the Support menu.
Can free-wheeling diodes be installed at the VFD output to protect against regenerative power ?
In any of the VFD's the free-wheeling diode in output will not help to protect the drive from motor. The freewheel diode is generally used in DC circuit for protection against reverse feeding. In VFD the regenerative power from motor must be dissipated through braking resistors or it should be properly inverted in to AC and should be fed back to the supply mains through regenerative braking units.