Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
Device Driver Matrix for Power Monitoring Expert (PME), StruxureWare Power Monitoring (SPM), and ION Enterprise
Issue
Which devices and device drivers are supported in PME, StruxureWare Power Monitoring (SPM), and ION Enterprise platforms?

Product Line
ION Enterprise 6.0 SP1
StruxureWare Power Monitoring 7.0.1
Power Monitoring Expert 7.2.2
Power Monitoring Expert 8.2
Power Monitoring Expert 9.0
Power Monitoring Expert 2020
Power Monitoring Expert 2021
Power Monitoring Expert 2022
Power Monitoring Expert 2023

Environment
Device Driver for Power Monitoring Software

Cause
Device support varies between the PME versions and platforms.

Resolution
The table below provides a list of the supported devices in the ION Enterprise 6.0 SP1, SPM 7.0.1, PME 7.2, PME 8.2, PME 9.0, PME 2020, PME 2021, PME 2022, and PME 2023 platforms.
Power Monitoring Expert 2023 (se.com)
Click on "Device Support Matrix"
Matrix link

Devices that are listed as "Installer" will require the installation of the device driver to add support for that device in the software.

PME 8.0 and 8.1 have been removed from the matrix.  Discuss upgrading to a recent version or request a custom driver be built.

Nomenclature
- Native means the device driver is available along with the software
- Installer means the device driver is available as a downloadable installer
- LE stands for Limited Edition driver which supports real-time registers and PC-based logging
- SE stands for Standard Edition driver which supports all features including onboard logs, waveforms,
control operation etc (provided such features are supported by the device)
- All drivers are SE type unless LE is mentioned against the driver name.

S stands for Standard device, which is the most advanced type of device
M for mid-range
E for entry-level

0.5M stands for half an M license. This is only used for particular device types like the Veris BCPM which is one physical device but is treated as two devices in the Management Console (one for each breaker panel).

- Newer versions of drivers are released as installers. If a newer version of a native driver is available, it will be indicated as "Installer" in this spreadsheet.

- 3rd party device drivers are available in the device drivers section of Marketplace in SEC (Power Solutions Community)