Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
This FAQ has been written for NEAL (North East Africa and Levant) region. If you are looking for information for another region, please select the correct country from the top-left dropdown in the page and 'Navigate to Browse FAQs' in the Support menu.
What Flange size is Schneider BCH servo motors offering ?

The BCH Servo motor has been designed to fit the requirement of any types of Machines, with 6 Different flange sizes 40 mm, 60 mm, 80 mm, 100 mm, 130 mm and 180 mm
BCH motor offer a wide choice of inertia from ultra low inertia to high inertia which provide the best match to different kind of machine :



1-Ultra low inertia motor: Power range is 0.1 ~ 0.4 kW, suitable for electronic equipment and small printing machinery.

2- Low inertia motor:Power range is 0.4 ~ 2 kW, suitable for textile and packaging machinery.

3- Medium inertia motor:Power range is 0.3 ~ 3 kW, suitable for material handling and machine tools.

4- High inertia motor: Power range is 2 ~ 7.5 kW, suitable for metal processing and printing machinery