Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
This FAQ has been written for NEAL (North East Africa and Levant) region. If you are looking for information for another region, please select the correct country from the top-left dropdown in the page and 'Navigate to Browse FAQs' in the Support menu.
How to upgrade Tesys T LTMR from version V2.4 to V2.5 or V2.6?
Please find the firmware version link below (Tesys T pack 8 - FW2.6) for download

Also find the attachment for the  procedure for LTMR upgrade .


https://www.se.com/products/ww/en/1500-contactors-protection-relays/1550-motor-management-system/1508-tesys-t/?p_url=http://www.ops-ecat.schneider-electric.com/ecatalogue/browse.do?el_typ=product&cat_id=BU_POW_1508_L3&prd_id=LTMR08MFM&scp_id=Z000&xtmc=LTMR08MFM&xtcr=1


In addition, The installation has to conform with the basic rules of Modbus communication

Improve Modbus network on site
1. install line polarization,
2. install end impedance,
3. connect of a zero volt reference between devices,
4. improve connections
5. Eliminate address conflicts.

LTMR Modbus User Manual
https://www.se.com/products/ww/en/1500-contactors-protection-relays/1550-motor-management-system/1508-tesys-t/?p_url=http://www.ops-ecat.schneider-electric.com/ecatalogue/browse.do?el_typ=product&cat_id=BU_POW_1508_L3&prd_id=LTMR08MFM&scp_id=Z000&xtmc=LTMR08MFM&xtcr=1

Schneider Electric Egypt and North East Africa

Attachment(s)
TesysT upgrade.pdf [911.51 KB]