Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
This FAQ has been written for NEAL (North East Africa and Levant) region. If you are looking for information for another region, please select the correct country from the top-left dropdown in the page and 'Navigate to Browse FAQs' in the Support menu.
Autotransformer starting of Motors (28.5 KW,...) ?

Autotransformer is a very old conventional and very expensive starting method, which is used very rarely after the introduction of Soft starters / VSDs etc.

On the small power motor, it is really very costly to implement this method as the autotransformer is an expensive part and we can achieve almost similar starting characteristics using the Star-Delta option.

For the lighter loads, the components need to be selected based on the current ratings.

It could be an option to use the type 2 coordination table for star delta starter for selection purposes only, but please refrain from referring to them as the Coordination table for Autotransformer starting as they are not tested validated, and certified on Autotransformer.