Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
This FAQ has been written for NEAL (North East Africa and Levant) region. If you are looking for information for another region, please select the correct country from the top-left dropdown in the page and 'Navigate to Browse FAQs' in the Support menu.
What is the MTBF (Mean time before failure) value for BMXP342020 ?
The following table indicates the calculated MTBF for M340 CPU’s. The values are in hours and years for continuous usage at 30 degrees C / 86 degrees F
Reference numberContinuous hours@ 30 degrees CContinuous years @ 30 degrees F
BMXP342020391864 (Hours)45 (Years)