Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
When do I change the Unit ID of Modbus/TCP equipment from 255 to a specific value in Vijeo Designer?

Issue

Customers that are having the Magelis communicate to a Modbus/TCP to Modbus/RTU devices.

Product Line

Vijeo Designer, Magelis HMI

Resolution

If you are using a Modbus/TCP to Modbus serial RTU Gateway device, each device on the serial network will have a Modbus server address associated with that device.  That Modbus server address is your Unit ID.