Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
What are the New Features of Vijeo Designer v6.2?

Here are the new features available when upgrading Vijeo Designer from V6.1 to V6.2:

· USB keyboard accessory support
· New Driver: Siemens 505 Ethernet
· RS485 Module support for Magelis iPC
· Templates to use in starting customer projects - especially ATV
· Registration: Vijeo Designer registration becomes mandatory
· Vijeo Design’Air and Air Plus support for Magelis iPC targets
· Vijeo Design’Air and Air Plus: Exclusive usage limited at Runtime, not at Buildtime
· Vijeo Design’Air Plus:
- New object: Message display object
-     Label for lamp