Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
This FAQ has been written for NEAL (North East Africa and Levant) region. If you are looking for information for another region, please select the correct country from the top-left dropdown in the page and 'Navigate to Browse FAQs' in the Support menu.
I have 140 CPU 671 60 in hot standby configuration. In the diagnostics Viewer (Unity Pro), the error symbols shows " ETH Device Failure" with Text ID 13010 ?

It is a 140CPU67160 known error V 2.70

Solution :-
kindly update the CPU Fimware & Copro to V3.20 & 3.10 ( firmware versions 3.20 must be used with Copro version 3.10 )


Find attached

Procedure related to firmware Upgrading a Quantum Hot Standby PLC refer Section 5 & Appendix 4
Kindly Refer section 5. Page no 50 follow same steps.

Schneider Electric Egypt and North East Africa

Attachment(s)
Quantum_Upgrade_Procedure.zip [1.57 MB]
140CPU67160.zip [1.01 MB]
140CPU67x6x_V320.zip [559.32 KB]