Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
This FAQ has been written for NEAL (North East Africa and Levant) region. If you are looking for information for another region, please select the correct country from the top-left dropdown in the page and 'Navigate to Browse FAQs' in the Support menu.
What is the amount of SF6 gas in 24 kV SF Circuit Breaker range.
In 24 KV SF Circuit Breaker range, the weight of the SF6 gas per pole for different Circuit Breakers is as follows:
  1. SF1 Type 1 – 49 grams
  2. SF1 Type 2 – 112 grams
  3. SF2 – 240 grams