Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
This FAQ has been written for NEAL (North East Africa and Levant) region. If you are looking for information for another region, please select the correct country from the top-left dropdown in the page and 'Navigate to Browse FAQs' in the Support menu.
What is the meaning of TROPICALIZED for Current transformers ?
The Tropicalized term is more related to the environmental conditions.
In fact it depends where you want to install the products (concerning Temperature and humidity characteristics).

The difference in Standard & Tropicalized CT is below :
Standard range: -5 °C to +55 °C, humidity < 95 %
Tropicalized range: -25 °C to +60 °C, humidity relative > 95 %.

Schneider Electric Egypt and North East Africa

Explore more
Product:
Users group

Discuss this topic with experts

Visit our community and get advice from experts and peers on this topic and more
Explore more
Product: