How can we help you today?

How to check the network by the PING command

On your PC, select the Window's [Start] button → [All Programs] → [Accessories] → [Command Prompt].
In the Command Prompt, enter "ping (the destination IP address)" and press ENT key.

PING Terminal Window

If it shows "0% loss", the network is normal. However, there is some problem if it shows "100% loss". In this case, check your network environment.

Schneider Electric Egypt and North East Africa

Users group

Discuss this topic with experts

Visit our community and get advice from experts and peers on this topic and more
  • Products Documentation
  • Software Downloads
  • Product Selector
  • Product Substitution and Replacement
  • Help and Contact Center