Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
This FAQ has been written for NEAL (North East Africa and Levant) region. If you are looking for information for another region, please select the correct country from the top-left dropdown in the page and 'Navigate to Browse FAQs' in the Support menu.
What does the ''Stop Check Back'' error in LTM R controller mean?
Stop Check Back
The Stop Check Back causes the LTM R controller to continuously monitor the main circuit to ensure no
current is flowing. The Stop Check Back:
-reports a Stop Check Back fault or warning if average phase current is detected for longer than 0.5
seconds without a Run command, or
-ends, when a Run command executes

Actions that can be taken :
Check the following:
- relay outputs
- all wiring, including:
·         control wiring circuit, including all electromechanical devices
·         power wiring circuit, including all components
·         load CT wiring.
After all checks are complete:
1-Reset the fault.
2-If the fault persists, cycle power and wait 30 s.
3-If the fault persists, replace the LTM R controller.