Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
How is the ATV12 programmed for a 4-20mA analog input on AI1?

Issue:
ATV12 programming AI1 for a 4-20mA analog input.

Product Line:
Altivar 12

Environment:
All models

Cause:
AI1 factory default is for a 0-5Vdc input.

Resolution:
Navigate to the AI1 Config menu using path ConF-FULL-IO-AI1-.  Set AI1t = 0A.  The input range is factory defaulted to 4-20mA, but can be changed with parameters CrL1 min and CrH1 max.