Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
What should the DC bus measure on an ATV312H...N4?

Issue:
How do I calculate / determine the DC bus value ?

Product Line:
Altivar 312

Environment:
All Altivar models and serial numbers

Cause:
Input rectifiers or DC bus have failed

Resolution:
The value of the DC bus voltage is dependent on the supply voltage.  The DC bus voltage should be approximately the value of the peak line supply voltage.  Example:  If the line supply voltage measures 480vac (RMS), then the DC bus will be 480 X 1.414 or approximately 678Vdc.

Schneider Electric Egypt and North East Africa