Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
What communication options (network protocols) are supported by the ATV312?
Issue:
ATV312  Communication Protocols

Product line:
Altivar 312

Environment:
All range  All serial number

Cause:
Ethernet TCP/IP

Resolution:
The communication protocol card that are available on the ATV312 are:
Modbus – Standard on the ATV312
CanOpen – Standard on the ATV312
Profibus – Option VW3A31207
CanOpen Daisy Chain - – Option VW3A31208
DeviceNet – Option VW3A31209
Early versions of the ATV312 documentation stated that Ethernet TCP/IP communication cards would become available as an option. This was incorrect. Neither Ethernet TCP/IP or Ethernet IP is currently available for this drive as an option card from Schneider Electric