Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
This FAQ has been written for NEAL (North East Africa and Levant) region. If you are looking for information for another region, please select the correct country from the top-left dropdown in the page and 'Navigate to Browse FAQs' in the Support menu.
Why to oversize the Softstarter used in a standard 400 V application, in case of using a bypass contactor?

In typical applications, may be the word oversizing could be not that accurate, because actually by bypassing the starter in a standard application & the motor always started from cold state, we can use the soft starter with one rating smaller in KW than without bypass.

Schneider Electric Egypt and North East Africa

Attachment(s)
ATS48 bypass wiring.pdf [51.68 KB]