This FAQ has been written for NEAL (North East Africa and Levant) region. If you are looking for information for another region, please select the correct country from the top-left dropdown in the page and 'Navigate to Browse FAQs' in the Support menu.
The ATS48 has 3 output relays, 2 of them are programmable (R1 & R3) thus can be configured, While R2 is assigned as end of starting relay to control the bypass contactor, it can not be configured
It is automatically activated when the motor complete the starting phase & no faults are present, it is deactivated when a stop command is sent & in the event of a fault.
To enable the function or disable it, this is done only by the wiring & R2 is already configured to do the function.
Attachments:
ATS48 Output Relays
Released for: Schneider Electric Egypt and North East Africa