Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
How do you setup a Jog on the ATV12?

Article available in these languages: Dutch

Issue:
Needs a jog input for the Altivar 12 drive.

Product Line:
ATV12, Altivar 12

Environment:
All models

Cause:
Using a logic input to Jog the motor.

Resolution:
Assign a Logic input under the Jog function (COnF > FULL > FUn > JOG).  Jog can be assigned to L1h, L2h, L3h or L4h.  The Jog function is a speed reference of 5Hz with 0.1s ACC and DEC.  This value cannot be adjusted.  If you need a jog faster than 5Hz, use a Preset Speed.

In order to Jog, the drive needs to have a direction command (Run Forward or Run Reverse input closed).

The Jog function is not compatible with PI Regulator.

Schneider Electric Egypt and North East Africa

Attachment(s)
BBV28581 May 2010 Jog function.pdf [177.44 KB]