How can we help you today?

How can you change the default home page background image on an EGX300?

Issue:
A user would like to change the default background image on the home screen of an EGX300? For example, a user may want to set the background image as a Company logo. The default background image for the home page of an EGX300 is shown below.

1

Product Line:
EGX300



Environment:
EGX300 User Interface

Cause:
A user does not know how to modify the default home page background image on an EGX300.

Resolution:
In order to change the background image on the EGX300 home page follow steps below:
1) Pick an image and rename the image to splash_custom. The image must be a JPEG  (.jpg).
2) Open my computer and in the address bar, type in ftp:\\XXX.XXX.XXX.XXX where XXX.XXX.XXX.XXX is the IP address of the EGX300.

2

3) You will then be prompted for log on information. The default log on information can be seen below.
Username: Administrator
Password: Gateway
4) Once logged into the FTP interface open the folder named "www", then open the folder named "logo". This is the location for custom home page background images.
5) Delete the file that is currently in use and drag your new image into the "logo" folder.
6) Open the EGX300 webpage and the home page background image will be changed.

Schneider Electric Egypt and North East Africa

Explore more
Range:
Users group

Discuss this topic with experts

Visit our community and get advice from experts and peers on this topic and more
Explore more
Range:

Need help?

Need help?

Product Selector

Product Selector

Quickly and easily find the right products and accessories for your applications.

Get a Quote

Get a Quote

Start your sales enquiry online and an expert will connect with you.

Where to buy?

Where to buy?

Easily find the nearest Schneider Electric distributor in your location.

Help Center

Help Center

Find support resources for all your needs, in one place.

  • Products Documentation
  • Software Downloads
  • Product Selector
  • Product Substitution and Replacement
  • Help and Contact Center