Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
When replacing and ATV58 by an ATV61, what is the LO (output contactor), what does it do?

Issue:
When replacing and ATV58 by an ATV61, what is the LO (output contactor)?

Resolution:
The LO is assigned to OCC. It is Output Contactor Command. The ATV61 does not have LO. The R1 and R2 relays on ATV61 are already being used in the circuit. Need to use any available contact off of the Run Command Relay and wire 24V through it to pull in the Drive Isolation contactor.

If this article does not answer your question, check out our FAQ database that has answers to more commonly asked questions:

Frequently Asked Questions - Schneider Electric (se.com)

If this FAQ did not solve your issue, you can call us at 1-888-778-2733 Option 2 and then 4 or e-mail us atdrive.products.support@se.comto create a case with our Technical Support Team.

If you are not located in North America, please contact your local Customer Care Center for assistance:

Support | Schneider Electric Global (se.com)