Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
This FAQ has been written for NEAL (North East Africa and Levant) region. If you are looking for information for another region, please select the correct country from the top-left dropdown in the page and 'Navigate to Browse FAQs' in the Support menu.
can we use MCCB NSX to protect a single phase load ?
we can use MCCB NSX to protect single phase load as we can use MCCB NSX  3P 2d which means that two poles are protected and we can connect the single phase load to one pole or we can connect in series connection