Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
This FAQ has been written for NEAL (North East Africa and Levant) region. If you are looking for information for another region, please select the correct country from the top-left dropdown in the page and 'Navigate to Browse FAQs' in the Support menu.
Why doesn't the LTMR Tesys T controller reset after the thermal fault?
If the relay is tripping on the Thermal overload fault, in this case it will need 30 to 40 minutes of the cooling time to RESET and restart.