Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
This FAQ has been written for NEAL (North East Africa and Levant) region. If you are looking for information for another region, please select the correct country from the top-left dropdown in the page and 'Navigate to Browse FAQs' in the Support menu.
What is the Main difference between the trip unit of Type Micrologic 2.2 and trip unit of type Micrologic 2.3 used with NSX MCCB ?
the Main difference between the trip unit of Type Micrologic 2.2 and trip unit of type Micrologic 2.3 used with NSX MCCB is in the usable rating range as explained in the following:

- Micro logic trip unit of type 2.2 is used with NSX MCCB of frame size ratings 100 A / 160 A / 250 A

- Micro logic trip unit of type 2.3 is used with NSX MCCB of frame size ratings 400 A / 630 A