Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
What is CFF fault on the ATV61 and ATV71 drives?

Issue:
CFF on the ATV61/71 drives

Product Line:
ATV61 and ATV71

Environment:
All models and serial numbers

Cause:
Option card changed or removed.

Resolution:
CFF is an incorrect configuration or the option card has been removed that will require the drive to be set back to factory default.