Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
How to add an ASCII string register type to a custom MDI device driver

Issue:
A user sees the following error ("Configuration error, The source is improperly configured or the requested register does not exist") in Vista when linking to an ASCII string register that is set up for a custom device in Modbus Device Importer (MDI).

Configuration error

Product Line:
Power Monitoring Expert 7.2
Power Monitoring Expert 8.x
Power Monitoring Expert 9.x
Power Monitoring Expert 2021
Power Monitoring Expert 2022
Power Monitoring Expert 2023
Power Monitoring Expert 2024

Environment:
Vista
Modbus Device Importer

Device Type Editor

Cause:
When an ASCII register is set up in the Modbus Device Importer, the register is not associated with the appropriate register type in the translator files.

Resolution:
*Warning: Take backups of any files prior to modifying them. Ensure the backups are in a location that will not be overwritten (i.e. the Desktop)".

  1. A user will need to manually modify the ION translator file for the device driver to assign the register to the appropriate format
  2. A user is only able to select the ASCII register format for a register added to an "External Numeric Manager"
Edit numeric variable
3. After adding the desired ASCII register, save and update the device driver, and locate the translator files and open the .xml and .ion files in a text editor
4. In the .xml file locate the ASCII register and make note of the ION handle number. In the example below the handle number is 135266305

ASCII register

5. Once you have identified the handle number for the ASCII register you will need to locate that handle number in the ION translator file. Make note of the register format highlighted in yellow below

Register Format
6. You will need to change this from "NumericVariable_Register" to "String_Register" as seen below

String Register change
7. After you have made this change save the ION file and restart Vista. The numeric object will now display the appropriate output from the string register
Vista
Note: Device Type Editor naming was introduced in PME 9.0 and replaced MDI