Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
Where are the basic wiring diagrams for an S-FLEX ?
Issue:
Basic wiring diagrams for an S-FLEX

Product Line:
S-FLEX 212

Environment:
All

Cause:
Needed for wiring and troubleshooting.

Resolution:
The standard wiring diagrams for units with and without the bypass feature can be found in the  S-Flex™ 212 Adjustable Speed Enclosed Drive Instruction Bulletin, document# 30072-451-83.
See attachments. Note that there have been design changes for bypass versions over the years.  The current bypass design is series E.

Schneider Electric Egypt and North East Africa

Attachment(s)
SFlex212 with Bypass series E.pdf [188.08 KB]
SFlex212 with Bypass series D.pdf [153.55 KB]
SFlex212 without Bypass.pdf [106.06 KB]
SFlex212 with Bypass.pdf [159.72 KB]