Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
This FAQ has been written for NEAL (North East Africa and Levant) region. If you are looking for information for another region, please select the correct country from the top-left dropdown in the page and 'Navigate to Browse FAQs' in the Support menu.
Using a capacitive sensor, How can I detect water level inside a tank ?
This can be done using a Glass tank for Example and using two sensors , First sensor is adjusted to detect the the glass and the second sesor is adjusted to detect the water .

Since glass has very low permitivity so the sensitivity of the first sensor needs to be increased , and the permitivty of water is very high so the sensitivity of the second sensor needs to be decreased (so as to detect water only ) .

The attached screen shot is an Example :