Issue:
Enclosed 22U dimensions.
Product Line:
8639/8638 22U, 22T, 22F soft starters
Environment:
Enclosed ATS22
Cause:
Needs dimensions on the 125HP 480VAC with no reversing isolation
Resolution:
You can find the dimension in the enclosed ATS22 22U install manual document 30072-453-26.
If this article does not answer your question, check out our FAQ database that has answers to more commonly asked questions:
Frequently Asked Questions - Schneider Electric (se.com)
If this FAQ did not solve your issue, you can call us at 1-888-778-2733 Option 2 and then 4 or e-mail us at drive.products.support@se.com to create a case with our Technical Support Team.
If you are not located in North America, please contact your local Customer Care Center for assistance:
Support | Schneider Electric Global (se.com)
Released for: Schneider Electric Egypt and North East Africa