How can we help you today?

PlantStruxure PES [V3.1 + SP1]: VBoxWrap.exe crashes

Goals and Symptoms

With PES installed in a virtual environment,
"VBoxWrap.exe" crashes during startup of the PES Server, whilst it is trying to start the embedded virtual machines.

as

Causes and Fixes

Enable ‘'Virtualization’' support on the CPU, via the BIOS of the HOST machine. The Nomenclature shall be different based upon the vendor of the PC like Virtualization technology. Virtualization, etc.

kb6