Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
What is the purpose of exporting the Vijeo Designer HMI target to an XML file format *.hmix?
Issue
What is the purpose of exporting the Vijeo Designer target to an XML file format *.hmix?

Product Line
Vijeo Designer, Intelligent Data Services (IDS) add-on

Environment
HMI Configuration Software in Windows

Resolution
The Vijeo Designer "export target to XML file" (*.hmix file extension) function is used to perform a static import into Intelligent Data Services (IDS)
IDS requires the *.hmix extension file that comes from the XML export of the Vijeo Designer project in order for the user to set up the different traceability options based on the variables in the *.hmix file.

Intelligent Data Services (IDS) is a Traceability Add-On package for Vijeo Designer which allows compliance for Food and Drug Administration (FDA) Title 21 CFR Part 11 (It requires that they implement controls, including audits, system validations, audit trails, electronic signatures, and documentation for software and systems involved in processing the electronic data that FDA predicate rules require them to maintain).

Schneider Electric Egypt and North East Africa

Explore more
Range:
Users group

Discuss this topic with experts

Visit our community and get advice from experts and peers on this topic and more
Explore more
Range:
  • Products Documentation
  • Software Downloads
  • Product Selector
  • Product Substitution and Replacement
  • Help and Contact Center