Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
This FAQ has been written for NEAL (North East Africa and Levant) region. If you are looking for information for another region, please select the correct country from the top-left dropdown in the page and 'Navigate to Browse FAQs' in the Support menu.
What are the advantages of using motor protection Circuit breaker over Fuse units in Motor Control panels?
Kindly be informed that in most common the motor protection Circuit breaker is always used for short circuit protection only. The fuse units protect against short circuit current also, but the main advantage for using MPCB is that it maintains the continuity and the sustainability of the supply and can be used for protection for a large number of operations according to the endurance and the reliability of the MPCB , rather than the fuse units that is used one time for short circuit and then needs to be replaced.