This FAQ has been written for NEAL (North East Africa and Levant) region. If you are looking for information for another region, please select the correct country from the top-left dropdown in the page and 'Navigate to Browse FAQs' in the Support menu.
For the DC control supply there is no need for the rectifier and the supply can be connected straight away across A1 (+ve) and A2(-ve).
The add on connectors supplied are not of any use when we use the rectifier with the LC1F800 type LX4F8** coils as an example
There are other versions of the coil for specific application different contactor references, where we use this rectifier and the provided add on connectors have defined implementation to facilitate the wiring.
Please be informed that the rectifier is only required to be used when the Coil control supply available is AC.
The AC supply is connected across the input for the the rectifier and the output from the rectifier is connected to the Coil . With +ve of the rectifier to the A1 of coil and -ve of the rectifier to A2 of the coil.
The add on connectors supplied are not of any use when we use the rectifier with the LC1F800 type LX4F8** coils as an example
There are other versions of the coil for specific application different contactor references, where we use this rectifier and the provided add on connectors have defined implementation to facilitate the wiring.
Please be informed that the rectifier is only required to be used when the Coil control supply available is AC.
The AC supply is connected across the input for the the rectifier and the output from the rectifier is connected to the Coil . With +ve of the rectifier to the A1 of coil and -ve of the rectifier to A2 of the coil.
Released for:Schneider Electric Egypt and North East Africa