Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
This FAQ has been written for NEAL (North East Africa and Levant) region. If you are looking for information for another region, please select the correct country from the top-left dropdown in the page and 'Navigate to Browse FAQs' in the Support menu.
what is the utilisation category for MCCB NSX , is it utilisation category A or B ?
kindly be informed that it's category A  ( you will find attached PDF mention that and the difference between the two cateogories

The standard defines two utilization categories, A and B; depending on breaker discrimination with upstream breakers under short-circuits conditions. Category A. Circuit breakers not specifically designed for discrimination applications.

Category B. Circuit breakers specifically designed for discrimination, which requires a short time-delay (which may be adjustable) and a rated short-time withstand current in compliance with the standard.

Compact NSX100 to 630 circuit breakers are category A, however, by design, they provide discrimination with downstream devices (see the Complementary technical information guide)

Schneider Electric Egypt and North East Africa

Attachment(s)
utilisation category definition.pdf [119.33 KB]