PlantStruxure PES [V3.1 + SP1]: PES V3.1 Licensing issue with VijeoCitect V7.3
Goals and Symptoms
If user installs PES v3.1 followed by installation of VijeoCitect V7.30, the PES license will be broken and the PES server will not start any more.
Facts and Changes
PES V3.1, Vjieo Citect V7.30
Causes and Fixes
PES V3.1 License will corrupt followed by installation of VijeoCitect(VJC) V3.0 because of the following reasons:
1.PES V3.1 installs Floating License Manager V1.0.0.0.
2. VJC V7.30 installs 1.0.2.0 which overwrites V1.0.0.0 without informing the user.
Steps to Recover the Corrupt License of PES V3.1:
1. Manually uninstall 1.0.2.0 (which will cause VJC Soft licensing to not be usable)
2. Re-install V1.0.0.0 from the PES installer package(PSXAS_V3.1_SP1_Official .ISO
\LicenseManagers\FloatingLicenseManagerSetup_PE.exe).
Note that this file will need to be copied on a read/write location, and not run from the iso (read only)
3. Finally, redo the license configuration described in the Process Expert Licensing Guide.
Released for: Schneider Electric Egypt and North East Africa
Need help?
Product Selector
Quickly and easily find the right products and accessories for your applications.
Get a Quote
Start your sales enquiry online and an expert will connect with you.
Where to buy?
Easily find the nearest Schneider Electric distributor in your location.
Help Center
Find support resources for all your needs, in one place.