PlantStruxure PES [V3.1 + SP1]: How to Customize GPL library
Goals and Symptoms
How to customize General Purpose Library(GPL) page templates in PlantStruxurePES.
Facts and Changes
PES V3.1SP1
Causes and Fixes
If user is using PES Native General Purpose Library (GPL), there may be need to customize the page templates provided by the library based on specific application.
Customization may mean changing appearance like adding customer logos or adding/modifying features or any others.
It is very important to understand that it is not recommended to modify directly the page template from the Native Library (sg2_include project).
If later,user have to migrate to a new version of PES, such methodology will lead to conflict.
The recommended methodology is only to create a new project template. This project template will have its page templates based on GPL Page templates.
Example illustration for correct methodology for GPL Templates Customization:
I. Step 1: Create New Template Project into Vijeo Citect
Import into your Vijeo Citect explorer ,the PES GPL Project Template (SGC_include2.ctz).
The CitectGPL project embeds all genies and pages templates used in PES GPL library.
2. The project template may be exported from the Content Repository in Globals->SGC_Include2.
User, then have to right click and save as.
3. In the Template, include the SGC_Include2 project. Doing this, user will be able to reuse all genies and symbol coming from the GPL library.
4. The need is to customize the page template behavior coming from GPL, but not modifying the template Menu. In order to avoid conflict between the SGC_include2 project and “MyTemplate” project, user have to remove the menu entries in “MyTemplate”
5. In “MyTemplate” Vijeo Citect Project, Delete all Menu entries: System->Menu Configuration or pagemenu.DBF.
Also Delete all entries from Alarm Servers, Report Servers, Trend Servers, I/O server: Servers-> Alarm Servers, ReportServers, Trend Servers, I/O server.
II. Step 2: Create New Page Template based on the GPL page template
1. Open from SGC_Include2, the Page template that user wanted to customize.
Use the page save as capability of Vijeo Citect (File -> SaveAs...) to save the page from SGC_include2 to “MyTemplate” project. The name of the page must be different from the one in SGC_include2 project.
2. Update the page ( Tools->Update Pages).
3. User can now customize his own page. Open it and do any change as per need. In illustrated example, Schneider logo has been added.
4. When it is done, create a backup of this project (Project->BackUp).
Note: If there is a need to change some genies from the template page, use again the same methodology: copy the Genie from SGC_include2 with new name, customize it and replace the old one in the new template page.
III. Step 3: Add Newly Created Vijeo Citect Template Project into PES
2. Add the Project template in the list of Included Project
IV. Step 4: Replace the Default PES Page Template by Newly created Page Template
2. In fact, PES will include the GPL SGC_include2 project in the Supervision project only when one genie of the GPL library will be assigned in a page.
3. To replace the templates from a page, user have to edit the page (or refine the Supervision project), right click on the page -> properties -> Appearance tab. User can then change the template by the one coming from his template project.
Released for: Schneider Electric Egypt and North East Africa
Need help?
Product Selector
Quickly and easily find the right products and accessories for your applications.
Get a Quote
Start your sales enquiry online and an expert will connect with you.
Where to buy?
Easily find the nearest Schneider Electric distributor in your location.
Help Center
Find support resources for all your needs, in one place.