Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
How do I disable the Webserver Configuration in ION Setup for the ION7330?

Issue
There is no option to disable the ION7330 webserver configuration access.

Product Line
ION7330

Environment
ION Setup 2.2
ION Setup 3.0

Cause
The default QuickION.cfg file does not account for the webserver config access.

Resolution
Placing the attached QuickION.cfg file in ...Schneider Electric\ION Setup\Tables\PML7330\ and reloading ION Setup will give the option to disable the webserver config access.

Schneider Electric Egypt and North East Africa

Attachment(s)
QuickIon.cfg [17.46 KB]