Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
what is the update cycle of digital input of 140ERT85410Z/140ERT85420 when it is located in the S908 remote drop
It will cost 2 PLC scan time to update the digital input of 140ERT85410Z/140ERT85420 when it is located in the S908 remote drop .

Schneider Electric Egypt and North East Africa

Explore more
Range:
Users group

Discuss this topic with experts

Visit our community and get advice from experts and peers on this topic and more
Explore more
Range:
  • Products Documentation
  • Software Downloads
  • Product Selector
  • Product Substitution and Replacement
  • Help and Contact Center