Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
What product line replaces the Class 8839 PowerGard CPA CPC CPD 18-pulse drives?
Issue:
Need a replacement for the Class 8839 PowerGard CPA CPC CPD 18-pulse drives?

Product Line:
PowerGard Class 8839

Environment:
All

Cause:
Replacement or new application

Resolution:
The PowerGard 18-pulse drive product line is obsolete.  The ATV680 and ATV980 product lines are the functional replacements. These are Active Front End units.

Schneider Electric Egypt and North East Africa

Explore more
Range:
Users group

Discuss this topic with experts

Visit our community and get advice from experts and peers on this topic and more
Explore more
Range:
  • Products Documentation
  • Software Downloads
  • Product Selector
  • Product Substitution and Replacement
  • Help and Contact Center