Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
What is the actual temperature on the heat sink if the ATV61 or ATV71 drives thermal is showing or reading 118%?
Issue:
Heat sink temperature on the ATV61/71 if thermal reading is 118%.

Product Line:
Altivar ATV61 ATV71

Environment:
All

Cause:
Wants to know how hot the heat sink is getting when the drives thermal is showing 118%

Resolution:
Approximately 100 degrees C is measred on heatsink.