Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
What is the ATS22 adjustment range for parameter In, Motor Rated Current?

Issue:
Motor Rated Current adjustment range on the ATS22.

Product Line:
Altistart 22 ATS22

Environment:
All models

Cause:
What range of motors can be used for a particular ATS22 model

Resolution:
The Motor Rated Current, In, is adjustable from .4x to 1.0x the ATS22 current rating, IcL.
In other words, it can be adjusted down to 40% of the ATS22's rating.

Eg: An ATS22C17S6U, rated 170A, has an In range of 68 - 170A.