Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
How to upgrade an older Web Designer application to support the latest exec firmware version

Issue
How to upgrade an older Web Designer application to support the latest exec firmware version.

Product Line
Ecostruxure Control Expert, TSXWMY100, 140NWM10000, BMXNOE0110, BMXNOR0200

Environment
Control Expert v14.1, Windows 10 version 1902 (OS Build 18362.30), TSXWMY100 v1.6, WebDesigner v2.33

Resolution
Web Designer does not allow the application target to be updated from an older version directly to the latest version.
In order to update the target version of the application, the update must be performed in sequenatial steps.

i.e., to update the target version for a TSXWMY100 application that is at version 1.6, the following needs to be performed:
1) Update the target version 1.7.

2) Update the target version 1.8.
3) Update the target version 1.9.


To update the target:
1) Click on the application name to highlight it.
2) Click on Target\Upgrade Target Version.

Schneider Electric Egypt and North East Africa

Explore more
Range:
Users group

Discuss this topic with experts

Visit our community and get advice from experts and peers on this topic and more
Explore more
Range:
  • Products Documentation
  • Software Downloads
  • Product Selector
  • Product Substitution and Replacement
  • Help and Contact Center