Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
This FAQ has been written for NEAL (North East Africa and Levant) region. If you are looking for information for another region, please select the correct country from the top-left dropdown in the page and 'Navigate to Browse FAQs' in the Support menu.
what is the expected maximum temperature rise within the terminals of Tesys D contactors?
All contactors are designed with respect to IEC 60947 (Low-voltage switchgears and controlgears - Contactors and Motor Starters) standard. This standard defines maximum permitted temperature rise depending on the contactor part. Please refer to the attached extract from IEC 60947.
Temperature rise means difference in temperature between the product part (e.g. terminals) and ambient temperature.
For example maximum thermal rise for copper is 60 K (see extract), which means if ambient temperature is 30°C, then maximum temperature of copper terminal can be 30 + 60 = 90°C. If ambient temperature is 40 degrees, temperature measured on copper terminal can be up to 100°C. (attached is the relevant page)

Schneider Electric Egypt and North East Africa

Attachment(s)
Temperature rise limits according to IEC 60947.pdf [88.27 KB]
Users group

Discuss this topic with experts

Visit our community and get advice from experts and peers on this topic and more
  • Products Documentation
  • Software Downloads
  • Product Selector
  • Product Substitution and Replacement
  • Help and Contact Center