Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
This FAQ has been written for NEAL (North East Africa and Levant) region. If you are looking for information for another region, please select the correct country from the top-left dropdown in the page and 'Navigate to Browse FAQs' in the Support menu.
Can we reverse line & load sides on NSX?
Yes, You can reverse feed LV432776 and most of the NSX range of MCCB's EXCEPT few models of R, HB1 & HB2 (attached catalogue excerpt)