Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
This FAQ has been written for NEAL (North East Africa and Levant) region. If you are looking for information for another region, please select the correct country from the top-left dropdown in the page and 'Navigate to Browse FAQs' in the Support menu.
What is the rated insulation voltage for MCCB of type NSX up to 630 A ?
The rated insulation voltage for MCCB NSX up to 630 is 800 V , this is the maximum voltage to be applied before voltage break down occurs