Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
This FAQ has been written for NEAL (North East Africa and Levant) region. If you are looking for information for another region, please select the correct country from the top-left dropdown in the page and 'Navigate to Browse FAQs' in the Support menu.
What is the range , type and application of ATV12

The Altivar® 12 drive is a frequency inverter for three-phase 200 to 240 V asynchronous motors rated from 0.18 kW to 4 kW.

Power ratings from 0.18 kW to 4 kW on three types of power supply: Two standard versions are available:
Drive with heatsink for normal environments and fan-cooled enclosure:
v 100 to 120 V single-phase, 0.18 kW to 0.75 kW (ATV12H...F1)
v 200 to 240 V single-phase, 0.18 kW to 2.2 kW (ATV12H...M2)
v 200 to 240 V three-phase, 0.18 kW to 4 kW (ATV12H...M3)

Drive on a base plate for mounting on the machine frame; the frame surface area
should allow heat to dissipate:
v 100 to 120 V single-phase, 0.18 kW to 0.37 kW (ATV12H018F1, P037F1)
v 200 to 240 V single-phase, 0.18 kW to 0.75 kW (ATV12H018M2, P..M2)
v 200 to 240 V three-phase, 0.18 kW to 4 kW (ATV12H018M3, P...M3)

Application :

Handling (small conveyors, etc.)
Packaging (small labelling machines, small bagging machines, etc.)
Pumping applications (suction pumps, centrifugal pumps, circulating pumps,mono-pump and multi-pump stations, etc.)
Machines equipped with a fan (air or smoke extraction, plastic film making machines, ovens, boilers, washing machines, etc.)