Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
What voltage level causes an Overvoltage Fault (OSF) on an ATV61 or ATV71 series drive?
Issue:
Overvoltage level on an ATV61/ATV71 that causes OSF

Product Line:
Altivar 61 and Altivar 71 series drives.

Environment:
All part numbers ending with M3XXX or N4XXX,  All serial numbers.

Cause:
N/A

Resolution:
- The over supply flag OSF FAULT is set when the drive is in the capacitor charging state and the dc bus voltage is higher than OSFH_Level.
- The over supply flag OSF FAULT is set when the drive is in the PWM deactivated state and when the dc bus voltage is higher than OBFH_Level.
- The flag OSF FAULT is reset when the dc bus voltage is lower than OSFL Level.
- The over supply detection is always activated and cannot be inhibited.


Schneider Electric Egypt and North East Africa

Attachment(s)
DC Bus Voltage levels.docx [55.61 KB]